What is the X1 part of the Sarix Thermographic camera part numbers represent?

Issue

Explanation of X1 suffix to the part number of the Sarix Thermographic cameras.

Product Line

Pelco Cameras

Environment

SP-ESTM314-X1 and other ESTM models.

Cause

Further clarification requested for Sarix Thermographic camera model numbers.

Resolution

X1 designates the cameras limited to 8.33 frames per second to meet United States government regulations when selling the thermographic technology overseas.

 

Sarix TM Series Thermography IP Cameras Specification Sheet