Difference between the PWRCRD-R and the PWRCRD-S power cords for DSSRV2.

Issue

What is the part number for the power cord of my country/region standard:  AU, EU, UK or US

Product Line

Pelco Video Management

Environment

  • DSSRV2
  • EN5516
  • PWRCRD-S-AR, -AU, -EU, -UK, -US
  • PWRCRD-R-AR, -AU, -EU, -UK, -US

Cause

Spec sheet list different type power cords.

Resolution

  • PWRCRD-S power cords are used for the DSSRV2 and ENC5516 encoder power supply.
  • PWRCRD-R power cords CANNOT be used on the DSSRV2 or ENC5516 encoder power supply.