How to re-align Optera cameras

Issue

The Optera camera sensors may require re-alignment.

Product Line

Pelco Cameras

Environment

Optera- IMM12018

Cause

  • The scene requires an adjustment to the factory default alignment.
  • In rare cases, the alignment can be thrown off after a firmware update

Resolution

There are 2 options:

  1. Factory defaulting the camera will trigger the default alignment.
  2. Log into the camera webUI and go to  http://yourCamerasIP/setup/imaging/alignment.
    • Here you will find options to Restore Factory Alignment, Automatic Alignment and Advanced Alignment Mode