Issue
After installing Continuum 2.0 SP1 problems are found with two of the System Default Listviewis.
- Errors This Month returns no results.
- Personnel_Expired Cards shows all cards not just expired cards.
Product Line
Andover Continuum
Environment
- Continuum 2.0 SP1
- Cyberstation
- ListViews
- Filters
Cause
Misconfigured Listview qualifier or filter.
Resolution
Errors This Month
The filter in the listview configuration is set to Root\OneMonthToNow. It should be set to Root\MonthToNow.
Personnel_Expired Cards
The listview qualifier needs to be configured as shown below.