How to Replace a damaged I/O Module

Issue

How to Replace a damaged I/O Module

Product Line

SmartStruxure Solution

Environment

Automation Server

AS

Cause

Hardware Failure

Resolution

  1. Remove the physical I/O device from the IO Bus and replace it with a physical I/O device of the same type.

    You can do this with the I/O Bus power on.

  2. In the IO Module Management Tool , verify that the physical device displays in the proper location.

  3. When finished, click Exit .

 

http://help.sbo.schneider-electric.com/Topics/show.castle?id=6660&locale=en-US&productversion=1.7.0rc&a=1