Adjusting the Focus on a Sarix Professional Series.

Issue

  1. Unable to locate the knob to adjust the lens on the IMP219.
  2. How to adjust the lens on the IMP219.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • IMP219
  • IMP Series
  • IXP, IBP series

Cause

Lens adjustment on a IMP Series camera is done uing the browser.

Resolution

Adjusting the Focus:

  1. Connect to the Sarix IMP camera using IE.
  2. Login to the Sarix IMP camera.
    Default user account is: admin / admin
  3. Select Settings
  4. Go to Imaging and select Focus to adjust the Zoom and Focus of the lens to the desired field of view.


     

NOTE: The focus can can also be adjusted by moving the zoom slider and using the Focus options in the live webpage.
              Focus adjustments is done exclusively with Web UI.

                  
 

 Zoom In: Click the button or click and drag the slider to zoom the lens in.

 Zoom Out: Click the button or click and drag the slider to zoom the lens out.

Quick Auto Focus: Click the button for the camera to start a quick search to find the optimal focal point for the scene.