Endura operations Rotate 180 degrees and Pan to zero will not work on all IP cameras will work with this command

Issue

The commands "Rotate 180 degrees" and "Pan to zero" will no work with most IP cameras including the Spectra HD and Spectra Enhanced

Product Line

Pelco Cameras, Pelco Video Management

Environment

When using Endura to control  IP cameras

Cause

The command that is sent out is teh same as preset 33 and preset 34. These are not set up in most  IP cameras. These are used in analog cameras and with an encoder.

Resolution

These commands are not in the IP Spectra series cameras. There is no work around