VideoXpert: How to setup a CMG as a local NTP Server.

Issue

It is highly recommended that VideoXpert be sync'd to a GPS clock for accuracy.
If a GPS clock is not available the time will gradually drift.
If time is not synced video displayed on the OpsCenter will start then freeze after a few seconds.

Product Line

Pelco Video Management

Environment

VideoXpert all versions
Meinberg NTP 

Cause

A GPS clock is unavailable and an alternative must be used.

Resolution

  1. Download Meinberg NTP and install it on the CMG, by default UDP port 123.
  2. Run the setup wizard.
  3. Click I Agree.
  4. Click Next.
  5. Click Next.
  6. On the Configuration Options page adjust your settings to match the screenshot below. The IP address listed below is an example. Use the IP address of your CMG here.
    NOTE: If your systems are configured for failover use the NTP server address here. 


     
  7. Click Next.
  8. Click Yes.
  9. Under "Use specific NTP servers" remove the word iburst. Then click File > Save. It should look like the below.


     
  10. Leave the defaults checked then click Next.
  11. A new account named "ntp" will be created. Input a password for this account then click Next.
  12. Click Finish
  13. Click the Start icon  on the lower left then the All Programs icon  then select Quick NTP Status.
  14. After 15 minutes an asterisk will appear next to LOCAL. 


     
  15. Proceed to install VideoXpert.