Issue
Do you have graphic pages and lines that do not update after an upgrade?
Environment
- I/NET Seven
- Windows PC
- Graphic pages
Cause
The following is the minimum requirements for any PC that is going to run I/NET Seven.
- Pentium IV (2.500 MHz).
- 1 GB RAM.
- 3 GB of available hard drive space. The Hard Drive should be 120 GB or more.
Resolution
There is one primary reason for this:
- Insufficient Memory: - Check the memory of the PC and verify that it is sufficient for the I/NET Seven Application.
- Explore into the hard drive C.
- Go to Properties and look at the physical description of the drive.