Evolution Grandeye 360 URL RTSP camera stream setting.

Issue

Unable to connect to the Evolution Grandeye 360 using VMS.

Product Line

Pelco Cameras

Environment

  • Evolution Grandeye 360

Cause

Incorrect RTSP URL address.

Resolution

H.264 video streaming:

4MP H.264 video stream:    rtsp://camera_IP_address/h264/video.sdp?camera=13
2MP H.264 video stream:    rtsp://camera_IP_address/h264/video.sdp?camera=25
1MP H.264 video stream:    rtsp://camera_IP_address/h264/video.sdp?camera=12
1/4   H.264 video stream:     rtsp://camera_IP_address/h264/video.sdp?camera=16

Note: Port 554 = H.264 rtsp stream