3rd Party Supported Models on IPCT01 version 5.92

Issue

What cameras are on the  supported list for the IPCT01 with version 5.92

Product Line

Other, Pelco Cameras

Environment

IPCT01

Cause

No 3rd party Supported list for IPCT01

Resolution

The following cameras are on the Supported list for the IPCT01

 

 

Brand

Support Models

ACTi

ACD-2100, SCD-2200, ACM-4200, AEK-1001B, SED-2120, SED-2120B, ACD-2200,

A-MTK

AM9730M, AM9539, AM323M, AM3519, AM6121

Arecont Vision

AV1000 series, AV5000 series, AV 8000 series

AXIS

205, 206, 207, 210, 211, 221, 231D, 232D, Q1755, P1311, P1344, P3344, M3014, Q6034

D-link

DCS-6815, DCS-6817, DCS-6818, DCS-6615

DVTel

CF-3111, CM-3111, CM-4021

DynaColor
IP Camera

NH060, NH070, NH101, NH210, NH061, NH221, NH062, NH102, NH073, V1, V2, V5, V6, VS201, W Series

DynaColor
IP PTZ

DH510e, DH610e, DH701e, DH811+e, NH720, NH820

UTC

TVC-MP1B-S, TVC-MP2B-S, TVD-MP1D-S, TVD-MP2D-S/E

IQinVision

IQ752, IQ511

Level One

FCS-3071, FCS-1131, FCS-1141

SIQURA

Siqura BC series, Siqura FD series

ONVIF

ONVIF comformance device                                                                             (compatible with ONVIF Comformance Test v1.02.2)

Panasonic

DG-NP304

Planet

ICA-230, ICA-312, IVS-110, ICA-151, ICA-750, ICA-150W, ICA-M220, ICA-107W, ICA-700, P400, ICA-HM131, ICA-HM126

Sony

SNC-CM120, SNC-CS20, SNC-DM110, SNC-DS10, SNC-DS60
SNC-DF85P, SNC-RX570P, SNC-DF40N/P, SNC-RZ25N/P

Sanyo

VCC-HD4000, VA-20LAN, VA-50LAN, VA-51LAN, VA-80LAN, VA-82LAN

ViVoTek

PT7135, IP7137(7000 series), IP 8161(8000 series),

Razberi Technologies

B200, B500, LP200, DV200, DV200L, D200, D200L, DVO200, DVO200L, BUO200L, PVO200-18