Power cord part number for POE75U-1UP .

Issue

The POE75U-1UP was not supply with a power cord.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • POE75U-1UP  
  • POE75U- 1UP-US

Cause

  1. The power cord is required but is not provided/shipped with the POE75U-1UP.
  2. The power cord is provided with the POE75U-1UP-US but it was misplaced or lost.

Resolution

Power cord part number:  PWRCRD-S-US  ....  PWRCORD, 117 VAC, STD US