Where to download CM9760-KBD Overlay sheet?


The CM9760-KBD function keys F1 through F24 are not easily identified.  A custom keyboard overlay template can be created and placed over the CM9760-KBD function keys.

Product Line

Pelco Matrix


  • CM9760-KBD All versions


A CM9760-KBD Overlay sheet is needed to construct intuitive labels for function keys F1 through F24


The CM9760-KBD Overlay sample sheet. can be downloaded here  The CM9760-KBD Overlay printing instructions can be downloaded here

Related Lessons Learned Articles

  • How to Setup Function Keys for the CM9760-KBD Intelligent Keyboard.  View Lessons Learned Article LL#13755 here
  • CM9700 Pelco System Manager Ver 9.0 and working with CM9700 Keyboard Templates.  View Lessons Learned Article LL#15207 here