Port logging functionality to log BACnet MS/TP traffic

Issue

It is not possible to use the Automation Server port log to view BACnet MS/TP communication

Product Line

SmartStruxure Solution

Environment

AS

BACnet

MS/TP

Cause

As of version 1.7 the BACnet plugin does not support logging MS/TP traffic to the com port's log file

Resolution

Note that if an attempt is made to start logging on a port configured for BACnet MS/TP no indication is given that the operation is not supported. The log file is actually created but nothing is logged to the file.

At the time of this writing no information was available about if/when this functionality maybe will be added.