Is the PT1260EX Pan/Tile explosion proof scanner certified for Zone 1 or Zone 2 standards?

Issue

Reference for Zone 1 or 2 rating for PT1260EX scanner.

Product Line

Pelco Cameras

Environment

PT1260EX

Cause

Missing refernence for Zone 1 or Zone 2 certifications in PT1260EX specification sheet.

Resolution

The PT1260EX pan/tilt series is rated with the follow certifications:

  • UL Listed (PT1260EX and PT1260EX/PP)
  • For use in Class I Devision I (Groups C and D) and Class II Devision I (Groups E, F, and G) hazardous locations (PT1260EX and PT1260 EX/PP)
  • Meets NEMA Type 4X standards

 

This system has not been certified for Zone 1, Zone 2 or any other ATEX international explosion proof rating standards.

Please see the specification sheet for further details.

UL Listed (PT1260EX and PT1260EX/PP)
• For use in Class I (Groups C and D) and Class II (Groups E, F, and G)
hazardous locations (PT1260EX and PT1260 EX/PP)
• Meets NEMA Type 4X standards