Esprit IP does not zoom out to 432X.


ES40E ES41E , will not zoom past 66X.

Product Line

Pelco Cameras


  • ES40E series
  • ES41E series


Electronic Image Stabilization is activated.

NOTE: • When electronic image stabilization is applied, digital slow shutter and wide dynamic range are disabled. Zoom, image resolution, and viewing angle are also limited when this feature is activated. • Electronic image stabilization cannot be used while in a preset that has motion detection activated.


To zoom past 66X,  Electronic Image Stabilization will be deactivated.