How do I program a power up action on a spectra Dome using a KBD300A

Issue

Programming  Power up action.

Product Line

Pelco Cameras

Environment

  • Spectra III, IV Series camera
  • Spectra Mini
  • KBD300A

Cause

Installation and Service

Resolution

NOTE: Not all models of Spectra CAmera offer the Power up feature.

Using the KBD300A, gain control of the camera

Tap 95 Hold preset for 5 Seconds

The Spectra dome menu will appear on the display.

NOTE: use the Joystick to navigate the camera menu, Iris Open to make selections or Enter any sub menu.
 

Once in the Spectra dome menu:

  1. Scroll down to Dome Settings then tap Iris open
  2. Scroll down to Power Up then press Iris open
  3. Press Iris open again to access the Power Up action selections.
  4. Verify the cursor/Arrow is now next to NONE (default power up action is NONE).
  5. Using the Up/Down arrows select the desired power up action you want the Spectra dome to do upon power up/reboot.
  6. Press Iris open to accept the selection.
  7. Scroll down to Back then press Iris open
  8. Scroll down to Back again
  9. Press Iris open to return back to the main menu.
  10. Scroll down to Reboot System and press Iris open
  11. Press Iris open to confirm system reboot.
  12. Verify the Spectra Dome resumes to the selected action in power up selection menu.