How many Oncam Grandeye Evolution 360's does the DSSRV/DSSRV2 support?

Issue

How many EVO 360 can be recorded on the DSSRV2?

Product Line

Pelco Video Management

Environment

  • DSSRV 7.5.609 or later
  • DSSRV2
  • EVO 360
    • EVO-05
    • EVO-12
  • DS ControlPoint

Cause

DSSRV recording and viewing of the EVO 360 using the DSSRV2.

Resolution

EVO-05 require Digital Sentry software version 7.5 and above.

EVO-12 require Digital Sentry software version 7.12 and above.


Recording
 
Motion Recording
DSSRV supports up to 6 Oncam EVO-05/EVO-12 cameras
DSSRV 2 Supports up to 8 Oncam EVO-05/EVO-12 cameras
 
Continuous Recording
DSSRV supports up to 8 Oncam EVO-05 / EVO-12 cameras
DSSRV 2 Supports up to 8 Oncam EVO-05 / EVO-12 cameras
 
 
Live Viewing Tested on DS CP-PC
 
Live Panoramic Decoding 
6 Oncam EVO-05 cameras*
4 Oncam EVO-12 cameras*
 

A DS-CPPC can view live video from up to 6 EVO-05 cameras, 4 EVO-12 cameras, or 2 Optera (IMM Series) cameras simultaneously (DS v7.12 or later).

Note: Tours not supported with Oncam/Optera cameras
 
*Viewing is based of the following PC specifications for the DS-CPPC.