What is the part number for an Active Display Port to HDMI converter for the DS-CPPC/DSSRV2?

Issue

What is the part number for an Active Display Port to HDMI converter for the DS-CPPC/DSSRV2?

Product Line

Pelco Monitors, Pelco Video Management

Environment

  • DS-CPPC
  • DSSRV2
  • Display Port (DP)
  • HDMI

Cause

No Display Port to HDMI adapter included with the DSSRV2/DS-CPPC literature kit.

Resolution

The part number for this adapter is DP2HDS.
Note: This is not a Pelco part number.

  • Converter type: Active
  • Max Digital Resolution: 1920x1200