What is the wavelength of the IL10 series cameras

Issue

What type of connection is the IL10

Product Line

Pelco Cameras

Environment

  • IL10-BA, IL10-BP Box Cameras
  • IL10-DA, IL10-DP Dome Cameras

Cause

Supported ethernet connections.

Resolution

The IL10 series are 100 BaseT.