Issue
When replacing the bubble on the IS or ICS cameras the picture becomes out of focus
Product Line
Pelco Cameras
Environment
- IS series
- ICS series
Cause
When focused without bubble on camera will be in focus until bubble is placed on, this is because of the curve of the bubble that the camera becomes out of focus.
Resolution
Will need to flip bubble around and focus camera through bubble to do focus, once focus is adjusted then place bubble back on camera.