Unable to use a Feature of Power Monitoring Expert due to license limitation

Issue

Unable to use a Feature of Power Monitoring Expert due to license limitation.   

Product Line

SmartStruxure Solution, Pelco Transmission & Power

Environment

Power Manager

Power Monitoring Expert

Cause

  1. Open the PME Management console
  2. Select Help>About
  3. You should see the active License Modules as shown below. You may or may not also see additional features that are part of the 90 day trial.  

Resolution

Contact your sales representative to purchase the additional licenses