The flicker correction mode on the Spectra Pro has a soft picture, if used for an outdoor scene

Issue

if you set the flicker correction mode to on in an outdoor scene the video will be soft and slightly out of focus. On an indoor scene the video does not show the issue.

Camera dispalys blurry video.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Sarix Professional
  • Spectra Professional Series
  • IBP, IMP, IXP Series

Cause

This has to do with how the flicker correction mode handles direct sunlight

Resolution

The flicker correction mode is used for when there are multiple lighting conditions, should not be used in an  outdoor mode. There are times it may need to be used at night