Issue
Can the Spectra Pro be programmed to call a preset location when an alarm contact is triggered?
Alarm contact trigger to preset.
Product Line
Pelco Cameras
Environment
- Spectra Professional - P1220
Cause
The Spectra Professional PTZ camera added support for this function in specific firmware.
Resolution
Yes, the "Go To Preset" event handler support was added in firmware version 5.10.34 and greater.
Spectra Pro Firmware Update v5.10.34
To find the most up to date firmware revision, refer to the Spectra Pro Product Page.