The Spectra Pro supports 1 connected alarm contact even though the hardware has 4 inputs.

Issue

The Spectra Pro has 4 alarm contact connects but currently only 1 contact functions.

Product Line

Pelco Cameras

Environment

  • Spectra Professional - P1220

Cause

Current firmware supports a maximum of 1 alarm contact connected.

Resolution

All four inputs are now supported with firmware v5.10.34. Please update using link - https://www.pelco.com/search?documentUUID=470fe8b6-a3b8-44cb-99dc-e79f509763ef&title=SpectraPro%20Firmware%20Update%20v5.10.34