Windows Error 1067 when starting the SigmaSvr in Windows Services

Issue

When SigmaSvr is started for then first time after a Sigma 4.08 install, a Windows error 1067 error appears

Product Line

Satchwell Sigma

Environment

Sigma 4.08

Cause

If SigmaSvr is started for then first time after a Sigma 4.08 install without the USB dongle plugged in the Sigma Sever may fail to start.

As a result a dump file will be created in the Sigma directory after each start attempt.

Resolution

  1. Before starting SigmaSvr, plug the Sigma USB dongle in.
  2. Let the driver install.
  3. Start the Sigma Server
  4. Delete the .dmp files in the Sigma directory.