Add-on versions required for use with Continuum 2.0 SP1

Issue

There are new versions of Continuum Reports, Archiver, Elevator Control, etc. that were updated by the Center of Excallence development team. These applications need to be upgraded prior to using Continuum 2.0 SP1 for sites that use these applications because of new memory mapping.

Product Line

Andover Continuum

Environment

Windows 7

Windows Server 2008

Continuum

Cause

Continuum 2.0 SP1 uses a new memory mapping scheme that allows for better use of large memory addressing. The Continuum Add-on applications needed to be updated in order to work properly, so each of the applications have an new version. Installers need to know which versions to update.

Resolution

1. Below is a list of Continuum Add-on applications and versions needed to work properly with Continuum 2.0 SP1

Prior to installing Continuum 2.0 SP1, you need to upgrade certain Continuum Add-on Applications with new versions. It is recommended that you be prepared to rollback to Continuum 2.0 should critical applications fail to operate after the upgrade to SP1. You can download new versions of the following Add-on Applications from The Exchange at this URL: https://ecobuilding.schneider-electric.com Search on 'continuumreports' and locate the application.

  • Add-on Application 2.0 SP1 Compatible Version
  • Access Groups 2.5.1
  • BioScrypt 4G V-Station Integration 1.12.1
  • CFR Extended Log Archiver Continuum Reports 23.0e
  • CFR Access Event Archiver Continuum Reports 23.0e
  • CFR Alarm Event Archiver Continuum Reports 23.0e
  • CFR Activity Event Archiver Continuum Reports 23.0e
  • Cogent MiY Integration 1.8.1
  • DVTel 6.x Video Integration 2.3.2
  • Elevator Control V2.6.6 2.6.7
  • EZ-GuardTour 1.2
  • EZ-Trap 1.9
  • Genetec Omnicast 4.8 Video Integration 1.1.1
  • Genetec Security Center 5.2 Video Integration 1.2.1
  • Personnel Data Importer Continuum Reports 23.0e
  • Salient Video Integration 1.3.1
  • Stentofon Integration 1.8
  • Video Inquire 1.9.1 
  • Customer-Specific Custom Applications
  • Contact COE.Support@Buildings.Schneider-Electric.com for upgrades for the following
  • customer-specific custom applications:
  • AckAlarm
  • Area Templates PIM
  • CADS
  • DVTel Alarming
  • Continuum-Excel
  • Elevator Control V3.x
  • Elevator Control V4.x
  • Elevator - EasyLobby Integration
  • Extended Log Exporter
  • PIM 2.0
  • ScanShell Scanner Interface
  • Surgard Integration
  • Vicon Video Integration
  • xTra 
  • Legacy Applications
  • Contact COE.Support@Buildings.Schneider-Electric.com for upgrades for the following legacy
  • applications:
  • Area PIM
  • Door PIM
  • Elevator Control V2.4
  • Elevator Control V2.5
  • Unlisted Application
  • AckAlarm
  • Area Templates PIM
  • CADS
  • DVTel Alarming
  • Continuum-Excel
  • Elevator Control V3.x
  • Elevator Control V4.x
  • Elevator - EasyLobby Integration
  • Extended Log Exporter
  • PIM 2.0
  • ScanShell Scanner Interface
  • Surgard Integration
  • Vicon Video Integration
  • xTra 

2. Download a pdf of this list click the following link:  Continuum Add-On Application version list