What temperatures do the EH16 enclosure heaters turn off and on?

Issue

No documented specification of EH16 enclosure heater temperature operation ranges.

Product Line

Pelco Cameras

Environment

All EH16 enclosure models with heater/blower option.

Cause

Require temperature operating range for the heater element. 

Resolution

The heater activates at 50 °F, + or - 8 °F. And deactives at 80 °F, + or - 5 °F.