How to make a script to call camera to remote monitors on Endura.

Issue

Camera Call up Script

Product Line

Pelco Video Management

Environment

  • WS5000 all versions

Cause

Basic Script making

Resolution

  1. Adding new Script
    Open Workstation and select Setup then Script





     
  2. Select Add and give the Script a Name


     
  3. Select Display  video then click on camera source


     
  4. Click In the field next to camera source



     
  5. The Select Device Box opens up now expand each location and select the camera repeat steps for Destination Monitor, Layout and Channel
    then select OK



    Also add Display Name and Alert text if applicable



     
  6. Now Select Apply at the bottom to save the Script