Move a PTZ to a preset based upon another cameras analytics using Digital Sentry.

Issue

Activate one cameras preset triggered from another cameras motion alarm.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry
  • Sraix firmware that supports motion detection.

Cause

  • Sarix Legacy
  • IM, ID, IE, IX Series cameras
  • Spectra IV IP, TXB-IP, TXB-N
  • Spectra HD
  • Esprit IP,
  • Sarix Professional
  • IMP, IXP, IBP series
  • Exsite IP
  • Spectra Professional
  • Sarix Enhanced
  • IME, IXE Series
  • Spectra Enhanced
  • Esprit HD

Resolution

  1. In DS create a zone.
  2. On the analytics tab add the camera that will fire off a supported behavior ex: camera sabotage.
  3. On the Cameras Tab add a camera  and choose the preset it will go to when the analytic triggers it.