Does Digital Sentry support the Oncam Grandeye Evolution 12MP IP camera?

Issue

Does Digital Sentry support the Oncam Grandey Evolution 12MP IP camera?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Evolution 12MP EVO-12
  • Digital Sentry 7.12.156 and above
  • DSSRV / DSSRV2
  • DS NVs

Cause

Purchase of a DSSRV2 and a EVO-12, verify compatibility.

Resolution

Yes, with the release of Digital Sentry software version 7.12.156 and above the Oncam Grandeye EVO-12 is supported.

 

Related Articles:
Where can I download the latest version of Digital Sentry software
How to install the Digital Sentry Software Suite on Digital Sentry HVR(s) and NVR(s).
How to add and configure an Oncam Grandeye EVO-05 to a Digital Sentry (DSSRV) recorder