Video is cut off when using wide angle lens inside an EH16 with SS16 Sun Shroud.

Issue

Video angle of View is blocked by  Sun Shroud.

Product Line

Pelco Cameras

Environment

  • EH16 Series Enclosure
  • SS16 Sun Shroud
  • 2.8 mm Lens

Cause

The use of wide angle lens and the Sun Shroud on an EH16 may  obstruct the angle of view.

Resolution

Not recommended for Wide angle applications without modification.

Work around: Cut Sun Shroud with hack saw: not recommended. May cause glare in some applications.

 

Related Topic:

How do I customize a Pelco product using the Special Modification Request (SMR) Process?