Indoor corner mount for IME and IMP Sarix IP cameras.

Issue

Is there an indoor corner mount for the Sarix IM Enhanced and IM Professional IP cameras?

Product Line

Pelco Cameras

Environment

  • IME Surface Mount Vandal-Resistant (-1VS)
  • IME Surface Mount Environmental (-1ES)
  • IMP Surface Mount Environmental (-1ES)
  • IMP Surface Mount Environmental with IR (-1ERS)
  • SMR
  • IMEP-VCM

Cause

Installing Sarix IME series IP cameras into elevators.

Resolution


This is available via a Special Modification Request, order using SMR 1-2D59HX