AS Password policy configuration grayed out

Issue

The automation server password policy is grayed out making it unavailable to make configuration changes. These password policy settings can be located in the Control Panel > Security and communication > Security settings area. 

Product Line

SmartStruxure Solution

Environment

  • StruxureWare Building Operation Enterprise Server
  • Workstation
  • Control Panel
  • Security and communication

Cause

When an Automation Server is attached to an Enterprise Server, all of the password policy configurations are inherited from the enterprise server. Therefore the AS settings cannot be changed. 

Resolution

The password policies of the Automation Server must be administered from the ES when it is connected to an Enterprise Server.

 

In order to make changes to the password policy settings in the Automation Server directly, it must be detached from the Enterprise Server.