Issue
Wanting to record locally on camera.
Product Line
Pelco Cameras
Environment
-
Spectra Pro Series
- P1220 models
-
Spectra Enhanced Series
- S6220 models
- S6230 models
- Spectra HD and IP do not support SD card
Cause
Which cameras support SD card recording.
Resolution
Spectra Pro:
Up to 32GB onboard; Micro SD, SDHC Compatible Capture 1–5–10 second video clips on camera sabotage, motion detection, or alarm input (accessible using FTP protocol); record video continuously using ONVIF Profile G.
Spectra Enhanced:
32 GB SD Card; Capture 1–5–10 second video clips on camera sabotage, motion detection, or alarm input; record video continuously in the case of network outage with option to overwrite; access video through FTP protocol and ONVIF Profile G