Is Pelco Mobile compatible with VideoXpert?

Issue

Pelco Mobile and VideoXpert compatibility

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • VIdeoXpert
  • Pelco Mobile

Cause

VideoXpert is a new VMS 

Resolution

Yes, you can add a VideoXpert system into your Pelco Mobile app. If you would like to Demo VideoXpert and Pelco Mobile functionality, you can use the following settings to add our Demo VideoXpert system.

IP/Host: 12.104.144.8(Core IP)
Port: 443
SSL: Make sure the checkmark is highlighted
Name: Enter the name of your system
Username: guest1
Password: demo1234