I can see the data when I preview the report but when I print nothing happens

Issue

I can see the data when I preview the report but when I print nothing happens

Product Line

TAC I/NET

Environment

I/NET Site

Cause

No printer is selected or the no printer option is checked.

Resolution

  1. From the Design View, right click in the blank portion of the Field View Area (this is the are under the Main Report tab).
  2. From the context menu select Designer > Printer Setup.
  3. In the upper left corner of the Printer Setup dialog confirm that the "No Printer" option is unchecked. This should allow you to select a printer. Please see the following screen captures:noprnt7rept.doc