What do the LED's on the Spectra Enhanced PTZ camera indicate?

Issue

There are LED lights which flash when the camera is operating, what do these LED's indicate?

Product Line

Pelco Cameras

Environment

  • Spectra Enhanced Series PTZ IP camera
    • S6220 / S6230

Cause

Verify the health of the camera.

Resolution