Zoom controls not available in WebStation when viewing a graphic

Issue

When viewing a graphic using WebStation, the zoom controls are not visible in the toolbar. Only "Reset zoom" is shown.

Product Line

SmartStruxure Solution

Environment

WebStation

Graphics

Zoom

Cause

The method of zooming a graphic in and out has changed at StruxureWare Building Operation 1.7.1. Prior to this a toolbar was available, but this has now been removed.

Resolution

To zoom the graphic in and out, the mouse wheel (scroll) is used.

The graphic can be positioned by dragging the graphic.

On a touchscreen, zooming is achieved using the pinched fingers method.

To reset the Graphic to a 1:1 ratio click "Reset zoom".