Issue
Unable to update LiveEvent View Window.
Environment
Continuum version 1.91 and above
Windows XP
Windows 7
Cause
Although MSMQ is enabled the MSMQ HTTP Port in the details must be enabled as well.
Resolution
To following steps should resolve this issue:
- Open Control Panel.
- Click Add Remove Programs and then click Add Windows Components.
- Select Message Queuing and click Details. ...
- Ensure that the option MSMQ HTTP Support is selected on the details page
- Restart the Live Event Viewer Window again and messages should be coming now
Windows XP Location:
Windows 7 Location: