Is the DX1100 Viewer supported on Windows 7?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Would like to install DX1100 Viewer onto a Windows 7 PC.

Product Line

Pelco Video Management

Environment

  • DX1100
  • DX1100 Viewer

Cause

DX1100 will not install or function correctly on a Windows 7 PC.

Resolution

The DX1100 is last supported on WIndows XP SP3, any newer version on Windows is not supported.

PC with the following minimum requirements:

  • Windows® 98, 2000, or XP operating system
  • Pentium® CPU (128 MB SDRAM and 400 MHz processing speed)
  • Matrox G400™ video card (16 MB memory)
  • Sound Blaster® -compatible card

DX1100 Manual download