What is the password for a NVR300.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

  • Confirming windows user and password
  • Confirming software user and password

Product Line

Pelco Video Management

Environment

NVR300

Cause

First time log in on the NVR300.

Resolution

Windows XP AS Administrator (administrator profile mode) or as NVR300 (user profile mode):

To log in to Windows XP as Administrator, Click Administrator and then enter the password. Note that the password is case sensitive.

The default password is 2921981@$. Then click the right arrow.The Windows XP desktop appears.
The default service password is pel2899100co (this will display the NVR-Config page.)