What is the purpose of the object called Object Creator?

Issue

If creating a new "Utility" in Workstation it is possible to create a object called " Object Creator". This object is not documented.

Product Line

SmartStruxure Solution

Environment

WorkStation version 1.7.1 and earlier

Cause

There is no documentation for this object, as it is an internal test object that should not be used in the field.
visible and if you use it wrong it will crash. In 1.8 it is removedIt’sIt’sIt’s actually a internal test object used to quickly 
create a folder structure. It shouldn’t be used as it isn’t supposed to be 
visible and if you use it wrong it will crash. In 1.8 it is removed
actually a internal test object used to quickly 
create a folder structure. It shouldn’t be used as it isn’t supposed to be 
visible and if you use it wrong it will crash. In 1.8 it is removedactually a internal test object used to quickly 
create a folder structure. It shouldn’t be used as it isn’t supposed to be 
visible and if you use it wrong it will crash. In 1.8 it is removedIt’s actually a internal test object used to quickly 
create a folder structure. It shouldn’t be used as it isn’t supposed to be 
visible and if you use it wrong it will crash. In 1.8 it is removed

Resolution

The object is removed in version 1.8