Spectra Enhanced and Optera camera do not require login to get into the web interface from the factory

Issue

No login required to get into camera web interface and to make setting changes

Product Line

Pelco Video Management

Environment

  • D6220
  • D6230
  • Optera

Cause

By default you can access the camera’s Web interface without authentication (due to ONVIF Profile Q compliance).

Resolution

Will need to set up a user profile on the camera to get a login for the camera.