The DX4700 / DX4800 displays Index of / when accessed using the web interface.

Issue

Connecting to the DX4700 / DX4800 using Internet Explorer or Firefox results in index page showing "Index of /".

 

Product Line

Pelco Video Management

Environment

  • DX4700 / DX4800
  • Internet Explorer
  • Firefox

Cause

Corrupt or failed firmware.

Resolution

Update or re-apply the latest firmware version.  Download the latest firmware release for the DX4700 / DX4800 (non HD units only) video recorder here
Refer to the following article for the update process: How to upgrade the DX4700 or DX4800 HVR software?