How far will the RC-LED remote work from the IR Illuminators.

Issue

Remote is not working when to far away.

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

  • IR850 series
  • IR940 series

Cause

Remote is to far away from IR Illuminator

Resolution

Remote maximum operating distance is 26 feet away.

 

Part number for Remote controller is RC-LED