Recall presets and deleating presets on CM9760-KBD.


How to recall presets from CM9760-KBD?

How to delete presets using CM9760-KBD?

Product Line

Pelco Matrix


PTZ camera

CM9760-KBD keyboard


Recall or remove presets using CM9760-KBD.


Recalling Presets

  1. Using the keypad, enter the preset number.
  2. Select PRST icon or press PRST/LOCK button.

Deleting Presets

  1. From the default menu, press DEF icon.
  2. In the define menu, press PRST icon.
  3. Enter the number of the preset you wish to delete in the keypad and press the DEL icon.