Issue
Which Xenta 101 stencil should be use in LonMaker?
Environment
Xenta 101-1VF, 101-1VFC, 101-2VF, 101-2VFC, 101-VF
Cause
Adding a Xenta 101 to a LonMaker drawing.
Resolution
Please use the following chart when deciding which Xenta 101 stencil to use in LonMaker:
Xenta Unit | Stencil |
101-1VF | 101 |
101-1VFC | 101 |
101-2VF | 101 |
101-2VFC | 101 |
101-VF | 101-VF |