VideoXpert: Accessory Server health check

Issue

Health Check

Product Line

Pelco Video Management

Environment

VideoXpert
Accessory Server

Cause

Health Check 

Monitoring Status

Resolution

To check the health of your Clustered Environment, simply go to the following URL: http://x.x.x.x:8080/haproxy_stats -> Replace x.x.x.x with the IP Address of the Accessory Server

EXAMPLE: http://192.168.5.100:8080/haproxy_stats


The username is that of the Accessory Server.  The default username is admin and the password is admin

1. Check the health of each Core Server using the legend provided at the top of the page. 

2. Check the health of each Gateway Server using the legend provided at the top of the page.

***Note the Bytes In and Out will give you a status of the server communication, the Status Column will show you the Up Time of that Server according to the Accessory Server.