VideoXpert: How to save and recall a tab.

Issue

A set of commonly used camera views needs to be created or recalled.

Product Line

Pelco Video Management

Environment

VideoXpert 1.10

Cause

By default there are no tabs.

Resolution

To create a Tab:
 
  1. Login to VideoXpert OpsCenter using the appropriate crednetials. The default is [Username: admin Password: your_specific_password].
  2. Click New then drag and drop a grid layout onto the monitor. Drag and drop cameras into each cell as needed.
  3. Click File then Save As on the upper left hand corner of the tab.


     
  4. Name the tab.



    At this point there are additional options.

    Save as global tab: This allows everyone on the system to use this tab.
    Collaborative tab: This shares the tab between two users. What one user modifies on his OpsCenter client will be reflected on the other OpsCenter client.
    Shortcut: The specified shortcut keys listed in the drop down can be assigned to call up this tab.
     
  5. Click Save.

     

To recall a Tab:

  1. Click Tabs then double click the appropriate one or drag and drop it onto a monitor.